Case Study
The Invisible Sleeve Holding the Electric Car Together
As automakers race toward 800-volt platforms, a quiet revolution in polymer science is helping protect high-voltage connections under extreme thermal conditions.
The wiring harness inside a modern electric vehicle is among the least glamorous components in the car. It is also among the most consequential. Stretching for miles through the chassis of a typical EV, branching into the battery pack, threading through the inverter, snaking around the motor, this nervous system of copper and insulation must endure punishing heat, corrosive fluids, and voltages that would have been unthinkable in a passenger vehicle a decade ago. And now, as the auto industry barrels toward an 800-volt future, the humble sleeve of heat-shrink tubing wrapped around those connections has become a frontline engineering challenge.
It is a challenge worth understanding, because the shift from 400-volt to 800-volt architectures is not an incremental upgrade. It is a structural reimagining of the electric powertrain one that promises charging speeds fast enough to rival the gas station experience but demands materials capable of surviving conditions that push well beyond the thermal envelope of conventional wire protection.
The 800-Volt Imperative
For most of the past decade, the 400-volt electrical architecture served as the industry's default. It was proven, it was manufacturable, and it worked. But it had a ceiling, and that ceiling was heat.
In a 400-volt system, delivering the kind of power required for ultra-fast charging in the neighbourhood of 250 to 350 kilowatts means pushing enormous current through the vehicle's wiring. Current generates heat. Heat demands heavier cables, larger cooling systems, and more robust insulation. The result is a thermal management problem that compounds at every junction, every splice, every termination point in the harness.
The elegant logic of 800 volts is that by doubling the system voltage, engineers can halve the current required to deliver the same power. The physics are straightforward: less current means less resistive heating, thinner conductors, lighter cables, and smaller cooling hardware. The market has taken notice. Industry analysts project the 800-volt EV architecture market will grow from roughly $13.8 billion in 2026 to over $36 billion by 2031, reflecting a compound annual growth rate above 21 percent. Several premium and volume automakers have brought 800-volt platforms to production. Including offerings from established European, Korean and Chinese manufacturers.
But halving the current does not eliminate the thermal problem. It relocates it.
Heat in New Places
The transition to 800 volts has introduced silicon carbide (SiC) MOSFETs as the power semiconductor of choice in traction inverters, the critical components that convert battery DC into motor AC. SiC devices offer roughly three times the thermal conductivity of their silicon predecessors, with switching losses low enough to enable smaller, denser inverter packages. The global SiC power device market reached between $2.7 billion and $5.8 billion in 2025 and is expanding at a pace of 19 to 27 percent annually.
hat density, however, comes with a paradox. While SiC inverters generate less total waste heat, they concentrate what remains into tighter spaces. Junction temperatures in 800-volt SiC modules can reach 175°C during sustained operation. The wiring and connection points surrounding these modules busbars, DC links, motor leads are designed to withstand not just conducted heat from adjacent components but also the radiant thermal environment of a tightly packaged powertrain.
Meanwhile, inside the battery enclosure, conditions present their own thermal signatures. Rapid charging cycles on an 800-volt platform can push cell temperatures into ranges that stress every material in the vicinity. And for wiring routed through the underhood or along the vehicle's undercarriage, the combination of powertrain heat, road-surface radiance, and limited airflow creates a sustained thermal load that legacy wire protection was never designed to handle.
This is the environment in which heat shrink tubing must now perform not as a passive wrap but as an engineered barrier against failure.
A Primer on Polymer Performance
Heat shrink tubing works on a simple principle: a polymer sleeve, manufactured in an expanded state, contracts tightly around a wire, splice, or termination when heat is applied. Once recovered, it provides electrical insulation, mechanical protection, and environmental sealing. The physics are elegant, but the chemistry is where the real engineering lives.
For decades, the automotive industry relied on standard radiation-crosslinked polyolefin tubing. These materials are cost-effective, widely available, and adequate for the thermal demands of a conventional internal combustion engine bay, with continuous operating temperatures of roughly 125°C, with periodic excursions somewhat beyond that. For a 12-volt or even a 48-volt mild hybrid system, polyolefin heat shrink was, and in many applications remains, perfectly sufficient.
But 800-volt architectures are rewriting the specification sheets. The sustained temperatures near inverters, DC-DC converters, and battery module connections now regularly exceed what crosslinked polyolefin can tolerate over a 15-year vehicle life. Automakers and their Tier 1 suppliers have turned to a class of materials that, until recently, were largely the province of aerospace and military applications: fluoropolymers.
The Fluoropolymer Leap
The fluoropolymer family PTFE, FEP, PFA, ETFE, and PVDF represents a step change in thermal and chemical resilience. The values below are typical published figures for these material classes; actual product ratings vary and must be taken from the applicable datasheet. PTFE-based heat shrink, for example, can sustain continuous operating temperatures of 260°C, with a working range that extends down to cryogenic levels. FEP and PFA offer similar high-temperature performance with the added advantage of optical clarity, which allows visual inspection of the covered connection without removal. PVDF sits at the lower end of the fluoropolymer spectrum, rated for continuous use at around 150°C, but brings superior mechanical toughness and abrasion resistance.
What makes fluoropolymers particularly well-suited to 800-volt environments is not just their thermal ceiling but the breadth of their resistance profile. These materials are highly resistant to degradation in the presence of battery electrolyte, transmission fluid, brake fluid, diesel exhaust fluid, and the glycol-based coolants now circulating through battery thermal management loops. In an EV, where the wiring harness may pass through or adjacent to multiple fluid circuits, this strong chemical resistance is not a luxury; it is a requirement.
The dielectric properties are equally critical. High-voltage heat shrink rated for 600 to 1,000 volts and above must maintain its insulating integrity not just at room temperature but at sustained operating temperatures, after thousands of thermal cycles, and in the presence of moisture and contaminants. Fluoropolymers retain their dielectric strength across an extraordinarily wide band of conditions, a characteristic that helps explain their longstanding use in aerospace wire protection, where the consequences of insulation failure are existential.
Beyond Temperature: The Multi-Threat Environment
Temperature, though, is only one axis of the problem. Automotive engineers designing for 800-volt platforms must also contend with a constellation of mechanical and environmental threats that interact with thermal stress in compounding ways.
Vibration is relentless. Wiring routed along the chassis or through suspension attachment points endures constant mechanical cycling that can abrade, chafe, and fatigue protective sleeves over hundreds of thousands of miles. Heat shrink tubing in these zones must resist abrasion not just when new but after years of thermal ageing, which can embrittle lesser polymers. Medium- and heavy-wall variants, often with shrink ratios of 3:1 or 4:1 to accommodate irregular geometries, are increasingly specified for these high-flex, high-vibration routing paths.
Moisture ingress is another persistent adversary. Adhesive-lined, or "dual-wall," heat shrink tubing addresses this by combining an outer polymer layer with an inner ring of hot-melt adhesive that flows during recovery and is designed to provide an effective moisture seal around the substrate. In 800-volt battery pack wiring, where even trace moisture can create conductive pathways with catastrophic consequences, adhesive-lined tubing has moved from a preferred option to a baseline requirement at many OEMs.
Then there is electromagnetic interference. The higher switching frequencies of SiC-based inverters generate EMI that can propagate through the harness and degrade the performance of ADAS sensors, infotainment systems, and vehicle communication buses. Shielded heat shrink tubing with a conductive inner layer or embedded metallic braid is finding its way into harness designs adjacent to high-frequency power electronics, adding yet another functional demand to a component that once had only one job.
The Standards Gap
One of the less discussed but increasingly urgent challenges in this space is the gap between existing standards and the real-world demands of 800-volt architectures.
The traditional standard governing automotive wire, SAE J1128, and its international counterpart, ISO 6722, were developed in an era when system voltages topped out in the hundreds and temperature classes clustered around 125°C. These standards are not obsolete; they remain essential for much of the vehicle's low-voltage wiring, but they were not written with 800-volt battery pack interconnects or SiC inverter outputs in mind.
Flammability testing, governed by standards like UL 224 VW-1, provides a floor for fire safety, but the halogen-free, low-smoke requirements increasingly mandated by European regulations and OEM environmental policies add another layer of complexity. Fluoropolymer tubing is inherently flame-retardant and produces minimal toxic off-gassing, which aligns well with these evolving requirements. Material selection must also account for evolving chemical regulations, including restrictions under consideration for PFAS/fluoropolymers, and should be assessed on an application-specific basis. But manufacturers must still navigate a patchwork of regional, OEM-specific, and application-specific qualifications that can vary significantly from one vehicle platform to the next.
Industry groups and standards bodies are working to close this gap. But for now, much of the specification work happens inside the engineering departments of individual automakers and Tier 1 suppliers, resulting in a fragmented landscape where material qualification can be as much about institutional knowledge as published test methods.
Manufacturing Under Pressure
The production side of the equation faces its own pressures. Fluoropolymer tubing is significantly more expensive than polyolefin, often by a factor of five or more, and its processing requirements are more demanding. Recovery temperatures for PTFE-based tubing can exceed 350°C, requiring specialised heat application equipment on the assembly line. The shrink ratios of fluoropolymer tubing are often lower (1.3:1 for some PTFE variants, compared to 2:1 or 3:1 for polyolefin), which limits its ability to conform to irregular geometries without custom sizing.
These constraints have driven a middle-ground approach at many manufacturers: use fluoropolymer tubing in the highest-stress zones inverter connections, battery module interconnects, motor lead terminations while retaining advanced crosslinked polyolefin for the vast majority of the harness where thermal demands remain moderate. The result is a tiered material strategy that optimises cost without compromising reliability at the critical junctions.
Newer formulations are beginning to narrow the gap. Radiation-crosslinked polyolefin blends with enhanced thermal stabilisers are pushing continuous operating temperatures toward 150°C, encroaching on territory once reserved for PVDF. Co-extruded tubing combining an outer layer optimised for abrasion with an inner layer engineered for dielectric performance allows designers to address multiple threat vectors in a single component. And advances in adhesive chemistry are improving the seal performance of dual-wall tubing at elevated temperatures, reducing the risk of long-term moisture ingress in thermally cycled environments.
The Road Ahead
None of this is visible to the driver. There is no product launch for heat shrink tubing, no press event where an executive unveils the latest fluoropolymer blend. But the engineers who design these systems understand that the performance envelope of the 800-volt electric vehicle is defined, in significant part, by the materials protecting its most vulnerable connections.
As the industry pushes toward even higher voltages 900-volt and 1,000-volt systems are already in discussion for commercial vehicles and next-generation performance platforms the thermal and electrical demands on wire protection will only intensify. The material scientists and polymer engineers working on the next generation of heat shrink tubing are, in a very real sense, working on the next generation of electric mobility itself.
It is a quiet, unglamorous kind of progress. It is also the kind that helps make electric mobility safer and more reliable.