Racing cars produce heat and vibration to levels that raise the eyebrows of our road-car colleagues!  So how do we go about making reliable solutions for our racing customers? Making parts smaller and lighter aids performance of a race vehicle, but understanding the dynamics of the vehicle and being trusted to solve performance and reliability challenges are what sets TE Connectivity’s Autosport teams apart from the rest of the motorsport industry. We want to be there making winning products and providing technical know-how to the world of racing for many years to come. As race teams can’t predict their updates (or how many times their vehicles will need spares because of accident damage), we need to be ready to support them as the need arises. We need to be able to ship parts around the world, as teams need them, so we developed a dedicated network of motorsport specific suppliers to meet this need.

Power Generation Solutions for Autosport Industry

CONNECTORS

Autosport is an arena that compiles harsh environment conditions - speed, temperature, oil and dust, vibrations, pressure. TE's DEUTSCH AS connectors help racecar teams face those extreme conditions.

SENSORS

TE with it's Measurement Specialties (MEAS) offer provides solutions for pressure, acceleration, force, torque, position, temperature and fluid properties. Over 80% of MEAS product supply is to custom designs in partnership with customers who expect the best sensor solutions for their unique applications. With advanced series of dynamic and static sensors, MEAS has the best technology offerings specializing in miniature sensors, light weight, shock/vibration testing and multi array scanners. Applications are wide and varied but extend to skid sensors, pitot, hydraulic/coolant pressures, chassis/hub vibration, bump stop force, pressure scanners for aero monitoring. All sensors are backed up with high reliability, extensive customer service and knowledgeable applications team to service customers' needs.

HEAT SHRINK MOLDED PARTS

Designed for demanding environments, TE's heat shrink molded products provide long-term protection against moisture ingress, corrosion, mechanical damage and extreme temperature.

WIRES AND CABLES

TE offers a wide range of Raychem high-performance wire and cable products that are designed to meet or exceed the most rigorous vehicle specifications.

RESISTORS

A resistor is a passive component that reduces voltage or limits the current flowing through a circuit. This component can also absorb energy and dissipate this energy in the form of heat. Its resistance to the flow of electrons is determined by the conductive materials with which it is built. The materials used in the composition of a resistor perform a critical role in enabling performance reliability and stability, particularly for high-voltage, high-power, high stability/accuracy, or high-current applications.

Insightful Resources on Power Generation

autosport-contact-us
Our Engineers are ready to help