Article
Utility-scale solar is growing fast. Projects are getting larger, schedules tighter, and sites more complex. At the same time, developers and EPCs are under pressure to preserve long-term performance while working with fewer skilled electrical labor resources than the market demands. <br>
Solar deployment is accelerating faster than the workforce available to build it. As a result, installation productivity, repeatability, and quality are becoming essential.
That's why the conversation around solar performance needs to go beyond modules and inverters. The way power is connected in the field is increasingly important to project success. In modern EBOS design, connection technology can influence schedule certainty, reliability, maintenance exposure, and long-term energy yield.
Real solar sites rarely match CAD drawings perfectly. Tracker shifts, drainage conditions, subsurface rock, land boundaries, and other civil deviations can all force layout changes during construction.
When projects rely on rigid, fixed-length assemblies, even small adjustments can lead to material waste, redesigning work, or schedule delays.
Solar IPC technology helps address this challenge by enabling tap locations to be adjusted directly on the trunk cable in the field. This allows installers to adapt to actual site conditions instead of forcing the site to match the original design.
This flexibility is not theoretical. At a 75 MW project, a 12 MW section had to be reconfigured after a burial site was discovered during construction. Using a SIPC-based approach, the EPC adapted the layout within the original timeline and budget without change orders or delays [1].
Adaptability delivers greater value when it is supported by long-term reliability. In utility-scale solar, even small weaknesses at a connection point can increase resistance, cause power loss, and lead to maintenance events over time[2, 3]. That is why sealing design and connection integrity are critical.
Our Solar IPC Technology uses sealed interfaces designed to limit water and oxygen ingress, helping reduce corrosion risk and maintain stable contact resistance over time.
This is supported by extensive validation, including IP68-rated sealing, 24-hour water-immersion testing, 2000+ thermal cycles, salt-spray exposure, UV and temperature cycling, and 100% electrical testing[4] before shipment. These are not just compliance checks. They reflect real environmental stress conditions.
Solar IPC technology enables multi-tap configurations that can reduce the number of connection points across large arrays while supporting efficient power collection.
As projects expand, preserving power becomes a system-wide challenge. Efficient generation is only one part of the performance equation. The system must also protect that power as it moves through the field. Connection design plays a direct role in minimizing losses and maintaining stable electrical performance.
TE's Solar IPC technology enables multi-tap configurations that can reduce the number of connection points across large arrays while supporting efficient power collection. Fewer connection points can also simplify installation and reduce potential sources of electrical loss[5].
In harsh environments (e.g., coastal, high-humidity, dusty, or high-temperature conditions), this becomes even more critical. Protecting electrical integrity at the connection point is essential to preserving yield and reducing long-term risk.
Labor productivity is becoming a defining constraint in utility-scale solar. With capacity growth outpacing workforce expansion, technologies that simplify installation and reduce reliance on specialized labor are increasingly valuable.[6]
Our Solar IPC technology simplifies installation to a single bolt - no crimping, no separate torque verification - so crews can complete connections quickly and keep the schedule moving. Connections can be completed in seconds, and teams have reported installing hundreds of TE´s Solar IPCs per day with small crews.[7]
Importantly, speed does not come at the expense of control. Visual verification features and shear-bolt installation logic help standardize installation quality and reduce field variability.
The takeaway is simple: the future of utility-scale solar will not be defined by modules and inverters alone. It will also depend on the quality, adaptability, and reliability of the electrical infrastructure connecting the system in the field.
As developers and EPCs look to build faster while managing project risk, connection technology is becoming a more strategic decision. One that directly impacts execution, performance, and long-term confidence.
Ready to take a closer look at your EBOS strategy? Read the trend paper or connect with our team to explore how Solar IPC technology can support your next project.
Designed for speed, Built to adapt, Made to last
SOURCES:
[1] TE Connectivity internal estimates based on implemented projects and customer inputs, as cited in the trend paper.
[2] Will Norman. "PV project power loss doubled in last five years - Raptor Maps." PV Tech, February 26, 2026.
[4] TE Connectivity. Solar IPC Assemblies SIPC.
[5] TE Connectivity. SOLAR IPC ASSEMBLIES SIPC. 2025.
[6] IRENA and ILO. Renewable Energy and Jobs Annual Review 2025. January 2026.
[7] TE Connectivity internal estimates based on implemented projects and customer inputs, as cited in the trend paper.