Discover our data connectivity solutions for industrial and commercial vehicles.
Download NowCommercial vehicle designers are increasingly introducing advanced functionality previously developed for passenger vehicles. Driver assistance and automation, infotainment options, 360-degree camera systems, high-speed V2V and V2I communication, and a wide range of essential safety features are now being integrated into commercial vehicles as well.
New technologies like these are made possible with a vehicle-wide set of sensors – including camera systems, radars/lidars, and more. These must be interconnected via a sophisticated network that can transmit high-speed data with low latency throughout the vehicle. Information gathered by these devices can then be processed using on-board electronic control units to create a complete model of the vehicle and its environment.
The transition to these types of technologies brings a whole new challenge for design engineers – who need to ensure that these vehicles perform even in the harshest environments. And that's where we come in.
We are specialized in the design and manufacture of the essential terminals and connectors which make these types of robust in-vehicle networks possible. We are an established leader in this market, leveraging our experience and proven performance in high-speed data, reliability in extreme environments, and collaboration with customers across the globe – to deliver solutions that are designed to meet the specific needs of truck, bus and off-highway applications.
Our design engineers take every element into account when developing and customizing new products – so everyone from your procurement and sales teams, right through to your customers and their operators, get exactly what they need to do their job out there in the real world.
Our specialized products all provide severe vibration and mechanical shock resistance, and some also allow for field maintenance in harsh environments such as those in which commercial vehicles operate. This includes situations involving dust, dirt, and moisture, and temperature ranges of -40°C to +125°C.
They can adapt to virtually any use, including radars/lidars, cameras, telematics units, antennas, onboard diagnostics, infotainment applications, head-up displays, and instrument clusters.
In industrial and commercial vehicles and machinery, designers must consider incorporating Ethernet systems in their designs now to be able to fully meet customer demands in the future.
The autonomous driving trend has long since gone beyond passenger vehicles. Ever more commercial and industrial vehicles are looking into introducing advanced functionalities.
Enabling advanced, data-heavy functionality means getting comfortable with integrating Ethernet into a mixed architecture.
Ensuring high-speed data transmission requires OEM designers to think more about components, placement and the impact of environmental conditions early in design.
It's time to look at Ethernet solutions for heavy-duty industrial and commercial vehicle applications that can transmit high-speed data with low latency, handling up to 1 Gb/sec of data.
With multi-function sensors and miniaturized connectors, embedded antennas and lightweight wire, engineers can build next-generation infotainment applications that enable smarter experiences for drivers, passengers, and pedestrians.
We are known worldwide for being a champion of innovation, with extensive application and system expertise – enabling the development of products that address future technologies. Find out more about some of our specialists, who are leading the field in Data Connectivity for Industrial and Commercial Vehicles.
Our products have been developed so that manufacturers of commercial vehicles – such as trucks, buses and off-highway applications – and marine craft are able to design the sophisticated systems that their customers are now demanding.
INFOTAINMENT
In addition to the entertainment and communication systems that provide driver satisfaction and enjoyment, this also includes access to information about systems that allow the driver to monitor and pilot the vehicle.
SAFETY
For any fleet manager, ensuring the safety of their employees is key. High speed in-vehicle communications enables a wide range of safety features – from lane departure warning, autonomous emergency braking and adaptive cruise control through to newer technologies such as lane keeping assistant, pedestrian detection, and even autonomous driving.
NETWORKS
This is the backbone of the vehicle, the underpinning infrastructure which makes all communication possible. Within the vehicle, from one vehicle to another, or between the vehicle and another location – whether that’s the owner’s depot or control centre, or even the manufacturer. The network provides for the reliability of the information transmission, making sure that the driver is fully informed about every aspect of his vehicle, at all times.
Our components have travelled up into space, and down into the deepest oceans – so whatever environment you need to operate in, you can be confident we’re up to the challenge.