load cells

Load Cell Technologies

Explore operating principles and core components that are key to selecting the right load cell for your specific applications.

Load cells are critical components in systems that measure force and weight. Their performance depends on the sensing technology they employ, as each uses a distinct physical principle to convert mechanical force into an electrical signal (or hydraulic pressure in some cases). These differences influence accuracy, durability, cost, and environmental suitability. 

Strain Gauge Load Cells

Operating Principle

The load cell body stretches or compresses when force is applied. Strain gauges bonded directly to the body respond by changing their electrical resistance. A bridge circuit detects these small resistance changes and produces a millivolt signal. Signal conditioning electronics amplify or digitize the signal to produce a calibrated output proportional to the applied force. Many industries—from manufacturing to material testing—depend on strain gauge load cells because they deliver high accuracy at a reasonable cost.

Core Components

  • Load cell body: A precision-machined element (beam or diaphragm) designed to deform elastically under load.
  • Strain gauges: Sensors bonded to the load cell body that change resistance as they stretch or compress.
  • Bridge circuit: A Wheatstone bridge arrangement that converts resistance changes into a measurable electrical signal.
  • Signal conditioning electronics: Amplifies or digitizes the millivolt signal into a calibrated output.

Capacitive Load Cells

Operating Principle

The sensing element deflects when force is applied, altering the spacing between two capacitor plates. Dielectric material insulates between the plates and influences the capacitance. The capacitance measurement circuit detects the change and produces an electric signal. Signal processing electronics amplify or digitize the output for display or control. Capacitive load cells offer high sensitivity and fast response, making them suited for precision applications such as laboratory balances and medical devices.

Core Components

  • Sensing element: A diaphragm or beam that deflects under load.
  • Capacitor plates: Two conductive surfaces whose spacing changes with applied force.
  • Dielectric material: Insulating layer between plates that affects capacitance.
  • Capacitance measurement circuit: Electronics that convert capacitance changes and convert them into an electrical signal.
  • Signal processing electronics: Circuits that amplify and calibrate the output for display or control systems.

Piezoresistive Load Cells

Operating Principle

The sensing element transfers force to semiconductor strain gauges, which respond by changing their resistance. The bridge circuit detects these changes and generates an electrical signal. Signal conditioning electronics amplify and calibrate the signal for output. Piezoresistive load cells respond extremely quickly, making them suitable for dynamic force measurements in automotive crash testing, robotics, and aerospace applications.

Core Components

  • Sensing element: A structure that transfers load to the semiconductor strain gauges.
  • Semiconductor strain gauges: Highly sensitive sensors that change resistance under stress.
  • Bridge circuit: Typically, a Wheatstone bridge that converts resistance changes into a measurable electrical signal.
  • Signal conditioning electronics: Instrumentation amplifiers, filters, and analog-to-digital conversion circuitry that produce a clean output signal.

Hydraulic Load Cells

Operating Principle

The load cell body transfers force to a diaphragm or piston, which compresses the fluid inside a sealed chamber. The pressure transducer or gauge measures the resulting pressure and converts it into a readable value proportional to the applied force. Hydraulic load cells require no electrical power and perform well in harsh environments, making them suitable for heavy-duty industrial weighing and remote locations.

Core Components

  • Load cell body: A housing that contains the fluid chamber and diaphragm or piston.
  • Diaphragm or piston: An element that transfers load to the fluid.
  • Fluid chamber: Filled with hydraulic oil or another incompressible fluid.
  • Pressure gauge or transducer: Measures fluid pressure and converts it into a readable value proportional to the applied force.

Technology Comparison

The table below compares key characteristics of the load cell technologies described above. Each offers distinct advantages and trade-offs. Strain gauge load cells strike a balance between accuracy, cost, and versatility, making them the most common choice for general industrial applications. Capacitive load cells excel in precision and speed but require controlled environments to maintain performance. Piezoresistive load cells are suited for dynamic force measurements where rapid response is critical, though they come at a higher cost and are sensitive to temperature. Hydraulic load cells, while less precise and slower, provide outstanding durability and independence from electrical power, making them suitable for harsh or remote environments. Selecting the right technology depends on the specific requirements for accuracy, environmental conditions, response time, and budget.

Characteristic Strain Gauge Capacitive Piezoresistive Hydraulic
Accuracy High
(±0.03–0.25%)
High
(±0.05–0.2%)
Moderate-High
(±0.1–0.5%)
Moderate
(±0.25–1%)
Response Time Fast Very fast Extremely fast Slow
Environmental Sensitivity Temperature & EMI sensitive Humidity & contamination sensitive Temperature sensitive Minimal (good for harsh environments)
Durability Good (with protection) Moderate (electronics sensitive) Moderate (fragile semiconductors) Excellent (rugged, no electronics)
Power Requirement Yes Yes Yes No
Cost Low - moderate Moderate - high High Moderate
Typical Applications General industrial weighing Precision low-force measurement Dynamic force sensing Heavy-duty, hazardous, remote

LOAD CELL FUNDAMENTALS

Explore the fundamental concepts that are important to understand load cells and discuss critical performance characteristics and environmental considerations.

READ MORE

LOAD CELL FORM FACTORS

Learn about the characteristics of the most common load cell form factors.

READ MORE