New low profile flexible printed circuit (FPC) connectors save valuable space with one of the lowest profiles in the market
These connectors save valuable space with one of the lowest profiles in the market at 1mm. They also improve customer assembly efficiency by having the actuator open at delivery, enabling one finger operation.
August 07, 2018
TE Connectivity (TE), a world leader in connectivity and sensors, today announced its new low profile flexible printed circuit (FPC) connectors. These connectors save valuable space with one of the lowest profiles in the market at 1mm. They also improve customer assembly efficiency by having the actuator open at delivery, enabling one finger operation.
The .5mm back flip version has a dual contact design which allows the connector to mate with the cable in two orientations. This enables more design flexibility and saves time during both design and installation.
The .3mm front flip version has additional FPC guidance features that reliably mate the cable to the fine pitch connector contacts, and helps the cable to be inserted into the housing correctly.
For more information on our FPC Connectors, please click here.