Mining in Latin America

Industries & Solutions

Mining Spotlight: Latin America

Home to 6 of the 15 most valuable mining operations in the world, and as the leader in copper production over the last 30 years, Latin America takes the spotlight.

Mine sites are extremely harsh environments. In the deepest mines, temperatures can reach 131°F (55°C). Mines in remote locations carry a very high cost of failure if products fail to perform reliably. These products need to withstand the most extreme temperature conditions. Bad sealing and water entry are the main causes of failures, so it is essential that products consistently hold up to constant environmental stress. 

Trucks Mining Iron Ore

25M

People directly supported by the global mining industry worldwide

150M

People indirectly supported by the global mining industry worldwide

$150B

Total amount of mined revenue from Latin America in USD; two-thirds from copper and iron ore

Largest Producer of Mined Metals in Latin America

Of the 473,819,000,000 kwh of energy used in Brazil per year, 18,952,760,000 kwh is used in the mining industry. Brazil is the third largest producer of iron ore with 364 million tons, with a projected additional 500 million tons over the next  years. As the world's biggest iron ore producer and the largest energy consumer in Brazil, Vale accounts for 4% of all of the energy absorbed. Vale is planning to expand production by another 90 million tons a year. 

Raw Iron Ore
Raw Iron Ore

474B

473,819,000,000 kwh used in Brazil per year

19B

18,952,760,000 kwh used annually in the Brazilian mining industry

Top Producer of Copper in Latin America

Chile is the number one producer of copper in Latin America, and produces 32% of all the world's copper. Exports of copper from Chile total $38.6 billion (USD), of the $45.3 billion (USD) of total mined exports. Chile is also the number two producer of mined metals in Latin America, and ranked first as the best Latin American mining investment. 18 million tons of iron ore were produced by Compania Aceros del Pacifico in 2016.

Raw Copper
Raw Copper

32%

Chile produces 32% of all world copper

$39B

Chile has $38.6 billion (USD) in copper exports

$45B

Chile has $45.3 billion (USD) in total mined exports

Second Largest Zinc Producer in Latin America

Mexico is the second largest zinc producer in Latin America – producing 630,000 tons, and is ranked fourth in terms of zinc reserves at 16 million tons. Ranked third as the best Latin American mining investmate climate, after Chile and Peru, Mexico outputs 15 million tons a year of iron ore from 4 main producers and more than 1000 small mines. 

Raw Zinc
Raw Zinc

630K

Mexico is the second largest zinc producer in Latin America – producing 630,000 tons

16M

Mexico is ranked fourth in terms of zinc reserves at 16 million tons

Ranked First in the World for Mineral Reserves

Peru has $2.2 billion (USD) in total mining revenue, with $55 billion (USD) invested in mining through 2016. 60% of all Peru's exports comes from mining production. Peru has 5-10 billion tons estimated iron ore resources, with planned expansion for increased production and iron ore expansion of an additional 60 million tons. Peru is ranked 2nd best Latin American mining investment climate, after Chile. Ranked third in the world’s zinc production, Peru produces 1.27 million tons. Ranked fourth in world’s copper production, Peru planned to double its copper production by 2016.

Open Pit Iron Ore Mine at Sunset

$2.2B

Peru has $2.2 billion (USD) in total mining revenue

5-10B

Peru has 5-10 billion tons estimated iron ore resources

$55B

Peru has $55 billion (USD) invested in mining through 2016