filter

Differential Pressure Transducers for Filter Monitoring

Differential pressure transducers can be used to monitor filters in various applications.

Differential pressure measurement is the difference in pressure between two points in a system.  For filtration applications, the upstream side [A] is positioned before the filter [B], whereas the downstream side [C] is after the filter. A differential pressure sensor can be used to monitor the cleanliness of a filter in either liquid or gas applications.

AST5400 differential pressure transducer across a filter

HOW IT WORKS

  1. The upstream pressure (commonly referred to as the line pressure or influent pressure) drives the media through the filter. A line is installed before the filter, as well as connected to the High side of the sensor.
  2. The filter then removes contaminants from the media.
  3. Next, the downstream pressure or effluent pressure, leads the media through the system with fewer contaminants than before. A line is installed on the Low side of the sensor in order to monitor the differential.
  4. When the filter is free of contaminants, the system will measure 0 PSI differential in pressure. As the filter becomes clogged, the pressure on the downstream side reduces, which creates a greater differential between the High and Low sides.While using the differential pressure sensor, the unit will offer a linear output signal based on the differential pressure.

EXAMPLE

A 100 PSI pump with a filter is installed to purify the water for drinking. If the downstream side in the system pressure drops to 80 PSI, the filter should be changed. With a 24VDC supply powering the sensor and a 4-20mA output signals elected, the sensor will be calibrated with a 100 PSI line pressure and 20 PSI differential pressure. When the system is operating with a clean filter, the output signal will be 4mA. As the pressure decreases on the downstream, the output signal will increase. Once the downstream pressure has been reduced to 80 PSI, the sensor’s output signal will reach the full scale of 20mA. When connected to a controller, the operator understands when to replace the filter.

BENEFITS

  • Oil free designs
  • High proof pressure ratings
  • High strength stainless steel or nickel alloy construction
  • Compact size
  • Line and DP pressure up to 5,000 PSI (350 Bar)
  • Increased resolution and accuracy
  • Simplified installation
engine
truck

APPLICATIONS

  • Water filtration for residential & commercial works
  • Fuel Filter Condition Monitoring for Diesel Engines
  • Diesel exhaust emissions monitoring
  • Transmissions
  • Natural gas scrubbers
  • Chiller systems
  • Oil / gas equipment