New Cages Improve Airflow, Can Help Reduce Costs
February 28, 2017
TE Connectivity (TE), a world leader in connectivity and sensors, today announced its Thermally Enhanced zSFP+ and zQSFP+ cages, which offer improved airflow through the cages, enabling better heat dissipation. These cages offer better thermal performance at a competitive price to most alternatives in the markets, and are ideal for any application that requires high-speed I/O transmission. The Thermally Enhanced zSFP+ and zQSFP+ cages offer:
• Better thermal performance – the best thermal performance of TE’s zSFP+ and zQSFP+ portfolio of products
• Better airflow – front-to-back and back-to-front airflow for cooler operation
• Lower costs – innovative and simple cooling enhancements can also lower operating costs
“As manufacturers move to higher internal speeds in their switches and other data communications equipment, they need I/O products that deliver 28Gbps performance without retaining too much heat,” said Melissa Knox, product manager of Data and Devices at TE Connectivity. “Our Thermally Enhanced zSFP+ and zQSFP+ cages improve thermal dissipation and are available at an attractive price point.”
View New Products
About TE
TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).