Extended USB Type-C line now offers dual-row SMT splash-proof connectors
New options offer a smaller footprint and further enhance rugged design.
May 24, 2016
TE Connectivity (TE), a world leader in connectivity and sensors, today announced its Dual Row SMT USB Type-C connectors, further extending its USB Type-C connector product line to include smaller mid-mount receptacles with a splash-proof option for added ruggedness.
USB Type-C connectors deliver audio/visual (A/V), data up to 10 Gbps and power up to 100W all through one connection. The small form factor features a reversible assembly that is adaptable to current USB types and a reversible interface for easy, reliable mating. TE’s USB Type-C designs deliver industry-leading EMI protection and enhanced printed circuit board (PCB) retention features. The new, splash-proof options make the Dual Row SMT USB Type-C connectors suitable for harsher environments in consumer and industrial devices. TE’s new receptacles also offer a space-saving 25% smaller footprint.
“With its ability to deliver data, power, and A/V in a single, compact connector, USB Type-C is gaining broad acceptance among electronics designers,” said Bowen Yu, Product Manager, TE Data and Devices. “By extending our USB Type-C product line with a Dual Row SMT configuration, we offer designers more flexibility to create compelling devices for their customers.”
About TE
TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).