Reduce Clutter with Double the Density
Meet the RJ point five connector coupler and plugs without pull tabs.
October 14, 2015
TE Connectivity introduces a new extension to its RJ point five product line that feature plugs without pull tabs to reduce clutter between routers and switches while still doubling the density of standard RJ45 jacks. As part of the extension, the new RJ point five coupler also offers easy integration with existing RJ45 plugs.
Features and Benefits
- Double the Density – Double the density of standard RJ45 connectors and cable assemblies
- Clutter Reduction – Absence of pull tabs reduces clutter between devices
- Design Flexibility – Coupler allows use of RJ point five connector with an existing RJ45 plug for easy design integration
About TE
TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).