Featured Product: New HD Card Edge Connector

Delivers high current density, low contact resistance

TE Connectivity debuts high density power card edge solution for data centers

January 25, 2018

HARRISBURG, Pa. – January 25, 2018 –  TE Connectivity (TE), a world leader in connectivity and sensors, today announced its high density (HD) card edge power connector, which delivers among the highest current density in the market to support high power supply applications.

TE’s new HD card edge connector delivers higher current than previous power card edge connectors at 25A/contact with low resistance, and supports 1500-2000W power supplies for data center equipment. With a maximum operating temperature of 130 degrees Celsius, the connector provides reliable performance in harsh environments. In addition, the signal pitch is 1.27mm (compatible with common industry PCB footprint designs), and the elasticity of the power/signal pins provides low mating force.

“Current density and power requirements in servers, switches and storage devices are increasing, and the industry demands solutions that can meet those needs in demanding environments,” said Bandy Yuan, product manager at TE Connectivity. “TE’s HD card edge connector is a solution that addresses the requirements of networking device manufacturers for next generation equipment.”

Visit the HD card edge connector landing page to learn more.

About TE

TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).

Find out more