New Product: ELCON Mini Power Solutions

ELCON Mini Connectors

Connectors Pack More Power in a Small Form Factor

TE Connectivity Announces ELCON Mini Power Connectors and Cable Assemblies

October 26, 2016

Harrisburg, Pa. – TE Connectivity (TE), a world leader in connectivity and sensors, today announced its ELCON Mini power connectors and cable assemblies—the latest innovation in its proven line of ELCON power solutions. The ELCON Mini family of products makes it easier for engineers to address increasing power demands, delivering a 400 Volt rating and up to 40 Amps per contact in a 2-position, 8mm high form factor that is roughly the size of a popular HDMI connector.

Power engineers and designers often need to be able to make power connections with limited available space and budget along with increasing power demands that can pose quite a challenge. ELCON Mini power connectors and cable assemblies are value engineered to address many power and space requirements with 2-, 3-, 4- and 6- (2x3)- position configurations, while providing a positive metal latch connection, low resistance, and highly reliable interface. Cable assembly solutions from TE also offer high-flex and customizable break-out options for easy routing and installation.

In addition to power input/output (I/O) and distribution applications, ELCON Mini connectors and cable assemblies are an internal wire-to-board power solution for the Open Compute Project (OCP) “Wedge” (top-of-rack) switches. The OCP is developing standard data center hardware designs that manufacturers can use to build highly compatible and scalable products with minimal development costs. Leveraging its decades of engineering experience and agility that come from offering one of the industry’s largest connector portfolios, TE is continuing to lead in providing power solutions for the OCP community.

“Our customers in a number of industries from data networking to medical and industrial need space-saving products that handle higher power levels and provide confident connections,” said Eric Powell, product manager, TE’s Data and Devices business unit. “Our ELCON Mini product family offers a mid-power solution in a broad range of attachments, configurations and cable assembly options to address increasing power and restricted space design requirements.” 

About TE

TE Connectivity Ltd. is a $13 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 78,000 employees, including more than 7,000 engineers, working alongside customers in nearly 150 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more

ELCON is a trademark.