New Product: DEUTSCH High Density Optical In-line Dry-Mate Connector

ILC-Connector-Pair

HIGH PERFORMANCE MULTICHANNEL FIBER OPTIC CONNECTORS

New in-line dry-mate connector offers increased environmental protection for marine fiber optics

February 02, 2018

TE Connectivity (TE), a world leader in connectivity and sensors, revealed today its new DEUTSCH high density optical in-line dry-mate connector. TE developed this multichannel fiber optic connector from reliable high pressure/high temperature (HP/HT) fiber optic technology that is backed by more than 30 years of performance in the field. It was designed to withstand harsh offshore environments and is ideal for applications that need maximum space and weight savings.


TE’s DEUTSCH high density in-line connectors offer a cost-effective solution for multichannel fiber optic management, packing 12 to 24 fiber optic channels (FO) in standard versions and up to 48 FO upon request. With operating temperatures between minus 30 and 121 degrees Celsius using the HT fiber, and bulkhead receptacles that are rated to withstand 450 bar (6,536 psi) of differential pressure, this multichannel fiber optic connector maintains stable performance during strain and temperature monitoring. Low insertion loss and back reflection (≤ negative 45dB) are achieved using angled physical contacts. In addition, the system maintains integrity in the face of flooding due to a dual sealing bulkhead receptacle.


“The new high density optical in-line dry-mate connectors are built from the same reliable technology used in multi-fiber optic HP/HT feedthrough systems, so engineers can expect a familiar interface that’s compatible with TE’s established DEUTSCH dry-mate connector,” said Jérémy Calac, product manager for marine oil & gas. “They are also optimized for offshore renewables systems, subsea flexibles and umbilical terminations.”
 

About TE

TE Connectivity Ltd. is a $13 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 78,000 employees, including more than 7,000 engineers, working alongside customers in nearly 150 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more