<rss version="2.0">
	<channel>
		<title>TE Connectivity Instrumentation and Medical Equipment News</title>
		<link>http://www.te.com</link>
		<description>TE Connectivity Instrumentation and Medical Equipment Product News Feed</description>


		<item>
			<title>Presenting the Ocean Applicator Series</title>
			<description>
  With the knowledge and experience of more than a half century designing and manufacturing world leading applicators and tooling, TE is taking terminal crimping to a new level. Using the time-proven HDM and HDI applicator platforms as a base and the innovation and improvements from the System III Applicator, TE has created the new Ocean Applicator series.&lt;br /&gt;&amp;nbsp;&lt;br /&gt;The lead and harness industry is more price and quality competitive than ever before. Crimping standards continue to be raised to higher levels of quality and repeatability and more is expected from application tooling. The Ocean Applicator series was designed specifically to exceed the requirements of today and meet the demands of tomorrow. By consolidating our applicator offering to this new applicator, TE can provide design consistency and tooling standardization. One of the major benefits is flexibility via a choice of feeding options: New and improved mechanical and pneumatic feeds combined with the innovative</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1920</link>
			<pubDate>Thu, 13 Oct 2011 00:00:00 GMT</pubDate>
		</item>

		<item>
			<title>New Miniature Snap-Action Pushbutton Switch Offers Longer Electrical Life</title>
			<description>&lt;p&gt;DARMSTADT, Germany -- Sept. 30, 2011 -- TE Connectivity has introduced a new miniature ALCOSWITCH Blue Series pushbutton switch. Its new internal snap-action mechanism combines compact dimensions with very fast switching and clear tactile and audible feedback indicating that the switch has been properly pressed. Applications cover power and signal. ALCOSWITCH Blue Series pushbutton switches are available in single- or double-pole, double-throw configurations (SPDT, DPDT) with push on/push off or momentary function. The internal contacts are brass with a silver inlay; optional gold plating is available for signal transmission up to 60mA @ 30VDC. The silver inlay contacts have an initial resistance of &#226;&#8240;&#164;10 milliohm at 125 VAC, at 1 A at 2 ~ 4 VDC. For the gold plated version the contact resistance is &#226;&#8240;&#164;20 milliohm at 100mA at 2~4VDC. Equipped with silver inlay brass contacts, the switches are rated for up to 250 VAC at 1.5 amps for European applications and for up to 125 VAC at 3 amps for North American applications. Due to the extremely fast contact travel, the silver inlay version's life is 25,000 cycles at load, and 50,000 cycles at load for the gold plated version. This compares to the UL requirement of 6,000 cycles at load. The higher lifecycle of the switch means that the lifetime of a valuable piece of equipment is less likely to be limited by its electromechanical control elements.&lt;/p&gt;</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1919</link>
			<pubDate>Fri, 30 Sep 2011 00:00:00 GMT</pubDate>
		</item>

		<item>
			<title>New Surface-Mount 2410 Fuses Provide High I&lt;sup&gt;2&lt;/sup&gt;t Characteristics</title>
			<description>&lt;p&gt;MENLO PARK, Calif. -- July 14, 2011 -- &lt;a href=&quot;http://welcomminc.createsend1.com/t/r/l/jullyhk/l/i/&quot;&gt;TE Circuit Protection&lt;/a&gt; announces the &lt;a href=&quot;http://welcomminc.createsend1.com/t/r/l/jullyhk/l/d/&quot;&gt;2410SFV&lt;/a&gt; family of 20 new AC/DC fuses featuring current ratings from 0.5A to 20.0A. The 2410 fuses help provide secondary-side circuit protection, conserve board space and reduce design costs in a broad array of high-voltage, high-current designs. Typical applications include home appliances (LCD TV LED backlighting, LCD TV CCFL backlighting) and LED lighting, as well as office automation, industrial and medical equipment.&lt;/p&gt;</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1910</link>
			<pubDate>Wed, 20 Jul 2011 00:00:00 GMT</pubDate>
		</item>

		<item>
			<title>Spring Finger Family Provides Better Internal Connection for a Wider Range of Mobile Devices</title>
			<description>&lt;p&gt;SHANGHAI, China -- June 28, 2011 -- As the demand for electronic devices continues to increase, so does the need for internal connections within these devices.  In response to this trend, TE Connectivity (TE), formerly Tyco Electronics, offers scalable spring fingers as well as a complete family of spring fingers to serve this surging need.&lt;/p&gt;</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1893</link>
			<pubDate>Mon, 27 Jun 2011 00:00:00 GMT</pubDate>
		</item>

		<item>
			<title>Power Line Filters to Comply with Strict Medical Standards</title>
			<description>&lt;p&gt;DARMSTADT, Germany &#226;&#8364;&#8220; April 29, 2011&#226;&#8364;&#8220; TE Connectivity (TE) has launched the Corcom HZ Series of power line filters. With current ratings ranging from 3A up to 30A and with low leakage current, the series complies with strict medical industry standards. The 30A version is TE Connectivity's highest amperage power line filters approved for medical applications. Corcom HZ Series filters offer solid attenuation from 10kHz to 30MHz and provide strong differential mode performance to effectively suppress line-to-line interference. The performance related to the small footprint of the devices &#226;&#8364;&#8220;  approximately 40% smaller than most competitive power line filters &#226;&#8364;&#8220; is unique. The small size of the filters increases the available space on the panel or box.&lt;/p&gt;

</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1875</link>
			<pubDate>Fri, 29 Apr 2011 00:00:00 GMT</pubDate>
		</item>

		<item>
			<title>Standard Range of Antennas Meets Diversified Customer Requirements</title>
			<description>&lt;p&gt;March 14, 2011 -- TE connectivity (TE) has announced a product line of standard antennas that can meet many customers needs.&lt;/p&gt;

&lt;p&gt;The new standard range of antennas offer low-profile, high-performance stamped metal, flexible printed circuit (FPC) and printed circuit board (PCB) embedded antenna solutions for single through penta band applications. These antennas are designed and manufactured to comply with stringent operating requirements and allow a wireless designer to select from a broad range of antennas with the frequencies that meet the needs of most wireless products. TEs global presence with manufacturing and design locations across the world enables TE to offer advanced antenna solutions with combinations of features in a variety of shapes and sizes, to suit customer unique wireless devices.&lt;/p&gt;

</description>
					
			<link>http://www.te.com/AboutUs/news/prodnews.asp?ID=1859</link>
			<pubDate>Mon, 14 Mar 2011 00:00:00 GMT</pubDate>
		</item>


	</channel>
</rss>