TE Connectivity
Illustration depicts female executives analyzing data on data chart indicating business performance.

Protecting Human-Led Tasks

Prioritizing human creativity could help maintain alignment and momentum.

Despite embracing AI as an innovation partner, 59% of engineers worry that their companies’ emphasis on efficiency and optimization means they are not doing enough to protect human creativity and support human-led tasks, compared to 47% of executives. These concerns are particularly acute in the Automotive and Data/Cloud Computing segments, where two-thirds of all respondents believe that their companies are prioritizing optimization over protecting human-led tasks.

Engineers also worry that the use of AI will limit their abilities to use their own judgment or creativity (40% vs. 27% of executives). This fear, coupled with differing priorities for measuring ROI, has made engineers more likely to question whether AI is delivering meaningful innovation (32%) than executives (18%).

To alleviate these concerns, businesses may need to communicate more clearly about where they expect to derive value from their AI efforts – and how they intend to preserve the engineer’s role as those efforts scale.

TE Takeaway

AI is fundamentally transforming how we approach both professional and personal challenges and opportunities. The underlying philosophy for effective AI adoption should position humans as the critical thinking leaders while leveraging AI as an intelligent personal assistant—essentially a digital extension of ourselves that amplifies our capabilities and effectiveness. The optimal approach treats AI as a thinking partner rather than a decision maker. This collaborative framework preserves human emotional intelligence and critical thinking in final judgments while harnessing AI's computational power for analysis, pattern recognition, and initial insights. However, we must remain vigilant and intellectually honest about AI's limitations. AI systems will make errors, produce biased outputs or provide incomplete analysis. Therefore, we must establish robust verification frameworks to assess AI effectiveness, cross-reference outputs with multiple sources and maintain the discipline to override AI suggestions when our expertise and judgment indicate different approaches.

Girish M K, Senior Manager, Engineering, AI Hub
Girish M K

Senior Manager, Engineering

AI Hub