Featured Product: New connectivity standard for IIoT implementation

SPS

TE Connectivity spearheads industry collaboration to establish new connectivity standard for IIoT implementation

The new standard easily integrates with existing Ethernet infrastructures to provide real-time data.

Schaffhausen, Switzerland

TE Connectivity (TE), a world leader in connectivity and sensors, recently led the establishment of a new Single Pair Ethernet (SPE) standard that enables companies to simply and cost-effectively connect devices on the network edge to make data-driven decisions in real-time. The International Electrotechnical Commission (IEC) 63171-7 standard creates broad industry consensus on a power-and-data hybrid format that easily integrates machines into a network and improves power distribution.
“Manufacturers often struggle to realize the advantages of IIoT because their networks can’t communicate from the cloud all the way down to an individual sensor on a machine,” said Eric Leijtens, global product management and managing director for TE. “This is why the new ‘-7’ standard is so critical. It helps us overcome that gap in data at the network edge by creating an industry-standard approach for connecting to physical assets in a production environment.”
As a founding member of the SPE Industrial Partner Network, TE led an industry consortium in recommending that M12 hybrid interfaces be specified under the new IEC 63171-7 standard. The standard now has the support of multiple trade groups and more than 80 companies. As one of the most common connector sizes in field-level applications, the M12 format easily connects to existing Ethernet infrastructure, replacing traditional fieldbus and analog solutions. With SPE implemented at the device level, manufacturers can realize transparent, IP-based communication replacing the current solutions that are expensive or have reduced transparency. The hybrid configuration in “-7” cables also provides increased flexibility to distribute power across the network, instead of the point-to-point connections required in power-over-data lines.

 

Other benefits include:

  • Long-term support. Standardizing on the M12 format enables manufacturers to work with multiple suppliers, providing for competitive pricing and a decreased risk of production downtime.
  • Reduced complexity and cost. SPE only requires one cable to deliver power and data through a single pair of wires, instead of two or four pairs, reducing cabling size and cost.
  • Increased data rate and power supply/ranges. The “-7” cable will enable power transmission up to 11kW/16A and high-speed data transmission up to 1Gbps/600MHz in one cable. It is excellent for high-power applications like DC servo drives, small three-phase drives, and many others.
  • Reduced electromagnetic interference (EMI). Separate data and power contacts reduce EMI.

About TE

TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions, proven in the harshest environments, enable advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With more than 85,000 employees, including over 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat and Twitter.

Find out more