TE News: TE Connectivity makes additional off-the-shelf components available

TE Connectivity makes additional off-the-shelf components available, streamlining customers’ time to market

Published

12/01/21

Media Inquiries

Katie Raymond
TE Connectivity
Tel: +1 717 985 2053
Email: k.raymond@te.com


Amy Wilson 
TE Connectivity
Tel: +1 717 985 2716
Email: amy.wilson@te.com

MIDDLETOWN, Pa.

Dec. 1, 2021

TE Connectivity (TE), a world leader in connectivity and sensors, is expanding its cable assembly portfolio to include off-the-shelf circular plastic connectors (CPC) and AMPMODU MTE cables. Off-the-shelf cable assembly solutions allow customers to quickly build and test prototype applications with products that have been time-tested in the market for more than 35 years, creating a one-stop shop for initial testing needs and providing customers durability they can count on in a shorter timeframe.


“Both CPC and AMPMODU MTE off-the-shelf standard cable assemblies allow for faster time to market, as customers will not need to separately order connectors, contacts, and cable clamps — instead, all components are included with the off-the-shelf solution,” says Tom Wess, TE product manager. “Furthermore, off-the-shelf solutions reduce installation time and offer a cost-effective option for cable assembly.”


Off-the-shelf cables help engineers and distributors identify quick and durable solutions for cable assembly prototyping needs, as TE can provide these components within one-to-two days. A shorter lead time contributes to a shorter time-to-market, which means distributors get products to customers far faster than they could without an off-the-shelf solution.

 

In addition to decreasing time to market, both CPC and MTEs provide rugged solutions designed to operate in harsh and space-saving environments. High-performance materials supply power input and output to and from almost any device, offering flexible options for quick prototyping and testing.

 

Key benefits of off-the-shelf CPC and AMPMODU MTE cables include:

CPC

  • Easy field repair
  • Heat-resistant, self-extinguishing material for added safety
  • Lightweight with space-saving features for harsh environment applications (IP65/57 rating)

AMPMODU MTE Cables

  • A strong positive latch helps to avoid unmating that often results from severe shocks.
  • Polarization feature helps to avoid incorrect mating, increasing safety for the operator.
  • Flexible options based on output and volume requirements/specific application needs.

About TE

TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions enable the distribution of power, signal and data to advance next-generation transportation, renewable energy, automated factories, data centers, medical technology and more. With more than 85,000 employees, including 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat, Instagram and X (formerly Twitter).

Find out more