New Product: QSFP-DD Connectors, Cages and Cable Assemblies

QSFP-DD Connectors, Cages and Cable Assemblies

New backward-compatible design enables easy upgrades for data centers

Unlike other 400G solutions on the market, QSFP-DD products are backward-compatible, which can provide an easy upgrade path from existing QSFP designs. TE’s QSFP-DD products leverage proprietary zipper fin heatsink technology allowing them to work cost-effectively in 15-18W applications.

July 18, 2019

TE Connectivity (TE), a world leader in innovative connectivity solutions for high-speed computing and networking applications, today introduced its new Quad Small Form Factor Pluggable Double Density (QSFP-DD) connectors, cages and cable assemblies, which address next-generation data center needs by increasing density through an existing QSFP form factor to reach speeds up to 400 Gbps. This 8 lane solution is designed for both 28G NRZ and 56G PAM-4 protocols, with a roadmap to 112G PAM-4 for future system upgrades.

 

Unlike other 400G solutions on the market, QSFP-DD products are backward-compatible, which can provide an easy upgrade path from existing QSFP designs. TE’s QSFP-DD products leverage proprietary zipper fin heatsink technology allowing them to work cost-effectively in 15-18W applications.

 

TE offers a broad QSFP-DD portfolio which includes 1x1 through 1x6 cages and surface mount (SMT) connectors on a 0.8mm pitch, along with various lengths and wire sizes of straight and breakout passive copper cable assemblies. Customer specific designs with different lightpipes, heatsinks and cable assemblies are also available, supported by TE signal integrity experts.

 

“As the world marches toward next generation connectivity in data center equipment, designers need new connector and cable assembly solutions to support this change,” said Zach Galbraith, product manager at TE Connectivity.  “We are excited to be one of the premier suppliers bringing QSFP-DD products to our customers, enabling 400 Gbps data rates through a single port. These products can provide much-needed flexibility to the industry’s end users, platform designers and system integrators.”

 

 

To learn more about TE’s QSFP-DD connectors and cable assemblies, click here.

 

About TE

TE Connectivity Ltd. (NYSE: TEL) is a $14 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more