New Product: DWFR Heat Shrink Tubing

DWFR Heat Shrink Tubing

Dual Wall Heat Shrink Tubing Meets UL VW-1 Requirement

DWFR tubing products combine flame-retardant and moisture-resistant capabilities for wide range of applications.

September 08, 2015

TE Connectivity (TE) introduces the DWFR (dual wall, fire-retardant) product line; its first dual wall heat shrink tubing products to be rated for the UL VW-1 flammability test specified by the UL 224 standard. The DWFR tubing products’ highly flame retardant polyolefin jacket and a thermoplastic inner adhesive wall provide excellent electrical insulation and mechanical protection. When properly installed, the tubing shrinks to create a moisture-resistant seal. The DWFR tubing products’ high heat-shrink ratios of 3:1 and 4:1 enable designers to use just a few tubing sizes across numerous applications – from home appliances to industrial controls to automotive. 

Features & Benefits

This tubing:

  • Is highly flame-retardant with UL VW-1 flammability rating
  • Provides excellent electrical insulation
  • Offers high shrink ratios for design versatility
  • Provides a moisture-resistant seal

Applications

Ideal for:

  • Appliances
  • Commercial electronics and communications
  • Automotive
  • Building equipment
  • Industrial machinery

About TE

TE Connectivity Ltd. (NYSE: TEL) is a $14 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more