New Product: Next Generation AMP+ Charging Cables and Inlets

AMP+ Charging Cables and Inlets

Smarter EV charging

“We now offer a complete charging system enabling the development of hybrid and electric vehicles. Together, with our proven experience in automotive connectivity systems and high-voltage applications, TE Connectivity actively drives green mobility and the supporting infrastructure.” - Luis Puras, Senior Product Manager for Hybrid and Electric Mobility Solutions at TE Connectivity

May 3, 2018

Bensheim, Germany – May 3, 2018 – TE Connectivity (TE), a world leader in connectivity and sensor solutions, launches its next generation of charging cables and inlets for hybrid and electric vehicles. The new charging cables are specifically designed to meet DIN EN 61851. Type 2 vehicle connector additionally meets IEC 62196. These standards define several types of on-board vehicle interfaces: type 1 for North America and Japan and type 2 for Europe with two charging modes at a wall power outlet or on high-performance charging stations.

TE Connectivity’s latest generation of AMP+ charging components enables significantly faster charging of hybrid and electric vehicles.

In compliance with the latest international charging standard IEC 62572, this AC charging solution can be plugged into any home power outlet with no specific charging infrastructure. The advanced integrated printed circuit boards monitor charging temperatures, while embedded Human Machine Interface (HMI) indicates fault and status. In addition, the enhanced housing design provides high impact, drop and drive-over resistance. These outstanding properties make the new AMP+ charging cable generation highly performing, easy-to-use and most robust.

Specifically designed to correspond with its charging cables, TE also launches its next generation combined charging system (CCS) inlet types that meet vehicle manufacturer requirements for plug-in hybrid and battery electric vehicles to charge in just a few minutes. 

 

 

About TE

TE Connectivity Ltd. (NYSE: TEL) is a $14 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more