October 26, 2015

Source: ElectroSchematics

"Wrist Mount Digital Altimeter"


"The barometric pressure sensor used in the design is the MS560702BA03-50 from TE Connectivity Measurement Specialties. It consists of a piezo-resistive sensor and a sensor interface IC. Its main function is to convert the uncompensated analogue output voltage from the piezo-resistive pressure sensor to a 24-bit digital value, as well as providing a 24-bit digital value for the temperature of the sensor. It is optimized for altimeters and variometers with an altitude resolution of 20cm."



Opens in a new window