pressure transducer

17-4PH versus 316L Stainless Steel

Comparison of two of the most common pressure transducer materials.

Stainless steel pressure sensors and transducers are most commonly manufactured from either 316L or 17-4 PH.  Both materials are relatively inexpensive, easy to machine in comparison to high strength nickel alloys, and offer good material strength, and good elasticity which allows for movement of a diaphragm. There are differences in their material properties that relate to both industrial and hazardous location applications that drive a preference for each material. While different types variations of these materials exist, TE has chosen the most basic and common forms used in the sensor marketplace today for comparison. The difference in iron content contributes to the magnetism and corrosion resistance. 17-4 PH stainless steel is magnetic and less corrosion resistant than 316L stainless steel. Standard 316L is slightly magnetic, but non-magnetic versions are available.  

Material Comparison

Composition 17-4 PH Percentage by weight (%) ASTM A693 316L Percentage by weight (%) ASTM A240
Carbon

0.070 max

0.030 max

Manganese

1.00 max

2.00 max

Silicon

1.00 max

0.75 max

Chromium

15.00 - 17.50

16.00 - 18.00

Nickel

3.00 - 5.00

10.00 - 14.00

Phosphorus

0.040 max

0.045 max

Sulfur

0.030 max

0.030 max

Copper

3.00 - 5.00

--

Columbium plus Tantalum

0.15 - 0.45

--

Nitrogen

--

0.10 max

Molybdenum

--

2.00 - 3.00

Iron

Balance

Balance

Material Strength

While the general understanding that stainless steel is has a high material strength is true when comparing it to a material such as plastic, the differences between types of stainless steel can be significant. When comparing 17-4 PH to 316L, it has a higher material strength. For many hydraulic pressure systems, where pressure surges and high cycles are common, 17-4 is more frequently used since it is a good spring material. Pressure sensors and transducers can be specified with proof (typically 2 times the rated pressure) and burst (typically 5 times the rated pressure) pressure ratings that are equal between the materials; yet there is a greater chance that 17-4 PH will measure accurately for a longer period of time when higher pressures and pressure transients above the rated pressure are present.

EB100 Miniature Pressure Transducer
M7100 pressure transducer
intrinsically safe pressure transducer
miniature pressure transducer

Compatibility

Stainless steel is stainless steel, right? When measuring liquids and gases, the type of pressure sensor material will be critical. 17-4 PH is used in various non-corrosive or mildly corrosive liquids and gases. Hydraulic fluid, brake fluid, fuels, and other standard industrial liquids will work well with 17-4 PH stainless steel. With higher nickel content, 316L stainless steel will work for these fluids in addition to many liquids and gases with more corrosive properties. For example, natural gas with low H2S content will need 316L to survive corrosion. Water (excluding salt water) is often considered a non-corrosive liquid, although 316L is preferred for pressure measurement. Various pH levels can cause 17-4 PH material to generate mineral deposits and clog process connections. Gases, such as hydrogen, require 316L material. Hydrogen ions are small enough to penetrate the grain structure of 17-4 PH stainless steel, thus breaking down the diaphragm over time as a result of embrittlement. For ultra-high purity applications such as semiconductor process equipment, 316L VAR (Vacuum Arc Melting) material is introduced to reduce non-metallic impurities. Further, material surface finish is put through a process called electro-polishing. This further reduces impurities from coming in contact with the liquid or gas by removing non-metallic imperfections as well as a small amount of the metallic surface. 

modern pump
offshore oil rig
car close up
orange forklift

Technology Comparison

Piezo Resistive Sensor Technology Manufacturing Process 17-4 PH 316L
Thin Film Metals are sputtered onto a stainless steel substrate. Yes No
Bonded Foil Strain Gage Strain gages are mounted to stainless steel diaphragm using epoxy or glass. Yes Yes
Chemical Vapor Depisition (CVD) Poly-silicon is chemically deposited onto a stainless steel diaphragm which is welded to a process connection after deposition. Yes No
Oil Filled

Silicon strain gages are encapsulated in silicone oil; pressure on a metal diaphragm compresses oil and changes sensor resistance.

No Yes
Thick Film

Thick film inks are screen printed onto metal

Yes No
Silicon Glass Fusion

Silicon strain gages are mounted directly to a one-piece stainless steel sensor through a glass firing process

Yes Yes

Summary

The technology used is an important factor. Certain technologies are limited in the material to which they can be applied. The strain gages applied to the diaphragm should match the thermal properties of the material to which it is applied. 17-4 PH stainless steel has a mean coefficient of thermal expansion of 6.0 x 10-6 in/in/°F with H900 heat treatment, whereas 316L ranges from approximately 9 to 11 x 10-6 in/in/°F. Technology such as thin film is limited to 17-4 PH because the temperature of the sputtering process is too high at the diaphragm. In summary, the difference in sensor material and technology can play a critical role in pressure transducer selection. Be prepared with information regarding the liquid or gas being measured and its application to help find the better option between materials. If neither 17-4 or 316L suffice, special alloys can be offered.