TE New Product Announcement: MATEnet Modular and Scalable Connectors

MATEnet Modular and Scalable Connectors for Automotive Ethernet

MATEnet Modular and Scalable Connectors for Automotive Ethernet

Infotainment solution designed to deliver top performance for harsh automotive environment.

October 04, 2016

TE Connectivity (TE), a world leader in connectivity and sensor solutions, today announced its new MATEnet modular and scalable connector for automotive Ethernet. The new solution provides the performance needed to transmit large volumes of data for transmit large volumes of data for infotainment, on-board diagnostics and more in vehicles.

TE’s MATEnet modular and scalable connector is designed for the harsh automotive environment and can transmit up to 1Gbit/s. Based on miniaturized standard automotive terminals, such as NanoMQS, Generation50, MCON 050 and 0.50 Series, MATEnet connectors represent a global terminal platform. In addition, they can be used with twisted pair (TP), unshielded twisted pair (UTP) and shielded twisted pair (STP) types of cable for Ethernet applications.

“The demand for more networking and bandwidth in vehicles continues to increase,” said Andreas Engel, senior manager of business development, Infotainment, for TE’s Automotive business. “Our new solution provides the performance needed to seamlessly handle more data while supporting the reliable and cost-efficient use of Ethernet in vehicles. TE is well positioned to support OEMs in their pursuit of a leading role in driving the connected car market.”

TE’s MATEnet modular and scalable connector for automotive Ethernet conforms with Ethernet IEEE specifications 100-BASE-T1 (100Mbps – Project IEEE802.3bw) and 1000 BASE-T1 (1Gbps – Project IEEE802.3bp). The new solution can also be customized, depending on the application or need. The new solution is ideal for infotainment, on-board diagnostics and 360° camera-system. 

About TE

TE Connectivity (NYSE: TEL) is a $12 billion global technology leader. Our commitment to innovation enables advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. TE’s unmatched breadth of connectivity and sensor solutions, proven in the harshest of environments, helps build a safer, greener, smarter and more connected world. With 75,000 people – including more than 7,000 engineers – working alongside customers in nearly 150 countries, we help ensure that EVERY CONNECTION COUNTS – www.TE.com

Find out more

Disclaimer

While TE Connectivity (TE) has made every reasonable effort to ensure the accuracy of the information in this article, TE does not guarantee that it is error-free, nor does TE make any other representation, warranty or guarantee that the information is accurate, correct, reliable or current. TE reserves the right to make any adjustments to the information contained herein at any time without notice. TE expressly disclaims all implied warranties regarding the information contained herein, including, but not limited to, any implied warranties of merchantability or fitness for a particular purpose. The dimensions in this article are for reference purposes only and are subject to change without notice. Specifications are subject to change without notice. Consult TE for the latest dimensions and design specifications.

 

MATEnet, NanoMQS und MCON are trademarks.