New Product: Cable Bundle Management System (CBMS)

CBMS

INSTALITE cable bundle management system (CBMS)

Organize and protect open wire bundles, with the benefit of substantial savings in weight and installation time when compared to traditional tapes and lacing.

July 26, 2016

TE Connectivity Ltd. (TE) (NYSE: TEL), a world leader in connectivity and sensors, announced the release of its new INSTALITE cable bundle management system (CBMS). Part of the Raychem product family, the CBMS provides a lightweight and highly flexible means of wire bundling and organization. The flexible sleeve accommodates a wide-range of cable sizes while still allowing for breakouts and transitions.

Used in commercial air, industrial, rail and defense industries, TE’s Raychem CBMS reduces the labor costs of taping or lacing. Instead, the flexible sleeve bundles cables and removes the need for taping of wires under overbraids. The sleeve was designed to save space, weight and power, and integrates with TE’s other INSTALITE products– like molded parts and lightweight braid – to create a complete lightweight system.

“The unique weave construction gives our Raychem CBMS much greater expansion and flexibility than traditional cable protection braids,” said Andy Poole, product manager, Global Aerospace, Defense & Marine, TE Connectivity. “It addresses the need for increased performance and reliability of systems while also reducing weight and installation times.”

TE’s Raychem CBMS is made from flame-retardant materials to perform in high temperatures and resists common fuels, oils and greases. The sleeving also provides abrasion-resistant protection to help prevent wire chaffing for a longer-lasting cable management system.
 

About TE

TE Connectivity Ltd. is a $13 billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 78,000 employees, including more than 7,000 engineers, working alongside customers in nearly 150 countries, TE ensures that EVERY CONNECTION COUNTS.

Find out more