New Product: TE's C-Lite Light Weight Cable Technology

c-lite cable

Light weight Cable Technology Holds Eight Leading Marine Classification Approvals

TE Connectivity (TE)'s C-Lite Cable Provides Reduced Size and Weight, Delivers High Performance

November 24, 2015

HARRISBURG, PA. - November 24, 2015 - TE Connectivity (TE), a world leader in connectivity, announces its C-Lite cable family of lightweight marine cables has received classification certification from the China Classification Society (CCS), making the C-lite family certified by eight of the top marine classification agencies in the world.

“The C-Lite family of cables are vastly small and light, letting customers do more with less,” said Mark Casselton, product manager, Global Aerospace, Defense, and Marine, TE. “And with TE’s new manufacturing facility in Kunshan, China, we are now able to better serve our customers in Asia with shorter lead times, helping them get to market faster.”

C-Lite cables use TE’s advanced materials technology to deliver a thin-wall insulation that dramatically reduces the size and weight of cables – without reducing the electrical or mechanical properties. From general power and lighting to communication, control and instrumentation applications, the C-Lite cable family is designed for use in a variety of commercial marine, offshore and military marine applications.

The C-Lite cables install up to 30 percent faster into a vessel or module compared to traditional cables, permit tighter bend radii and enable smaller cable trays and ancillaries, allowing more equipment to be connected within the same space. The thin-wall technology uses low-smoke and zero halogen wire and cable – which emits lower levels of toxic gases and generates considerably lower levels of smoke so that visibility is preserved in an emergency. The highly flame retardant cables are resistant to oils, solvents, fuels and petroleum mud.

In addition to the recent classification certification from CCS, TE’s C-Lite family of high-performance lightweight marine cables are certified by seven other leading marine classification approvals, including: ABS (American Bureau of Shipping), BV (Bureau Veritas), DNV (Det Norske Veritas),GL (Germanischer Lloyd), KR (Korean Register of Shipping), NK (Nippon Kaiji Kyokai) and RMRS (Russian Maritime Register of Shipping).

For more information on TE’s C-Lite cables, contact the Product Information Center at 1-800-522-6752 or visit our website.

Learn more about TE’s advanced connectivity solutions for the Aerospace, Defense and Marine industries.

C-Lite, TE, TE Connectivity and the TE connectivity (logo) are trademarks of the TE Connectivity Ltd. family of companies.

About TE

TE Connectivity (NYSE: TEL) is a $12 billion global technology leader. Our commitment to innovation enables advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. TE’s unmatched breadth of connectivity and sensor solutions, proven in the harshest of environments, helps build a safer, greener, smarter and more connected world. With 75,000 people – including more than 7,000 engineers – working alongside customers in nearly 150 countries, we help ensure that EVERY CONNECTION COUNTS – www.TE.com

Find out more