• English

Quareo - CPID


What Makes Quareo Unique?

Quareo Technology was developed in response to customer demand for visibility to the part of the network that has always been invisible: The physical layer.

Quareo Technology is a genuinely revolutionary connection point identification technology that brings managed connectivity to the physical layer of the network.

Consider the following: For the first time ever in the physical layer, you now have instant, automatic and accurate information that you've never had at your fingertips before. And imagine what you can do with that information.

Quareo's solutions feature unique Connection Point Identification (CPID) technology, enabling an automatic, accurate, and real-time view of a network, from the data center all the way to the desktop.

Connection Point Identification technology is very unique. It incorporates an integrated circuit placed right on a standard form factor connector, allowing for something that is very akin to a MAC-like ID--placed on the A and A-prime ends of the cable. This provides full accountability for each connection point within the network.

Security in today's networks is an extremely important topic. Many enterprises have remote facilities, either within the same geography or remote geographies. For the first time ever, Quareo provides the ability to a network administrator to instantaneously detect an unauthorized breach in the physical layer, and to take appropriate measures to respond. If an alien device was introduced into the network, for the first time, the 'man in the middle' attack can be viewed. Quareo technology tells the software and the network management personnel that the network was disconnected, and that even while the logical connection is back up, there is something else in the middle. Quareo provides a level of security that was not possible before.

Availability in today's networks is also a critical issue. For example, in a 10 Gig copper link, if someone inadvertently deploys a 1 Gig rated patch cord, today's network administrator can spend countless hours trying to troubleshoot root cause of that problem. Because of CPID technology, the network administrator can be informed instantly of that 1 Gig link being deployed in that channel, allowing appropriate measures to be taken immediately, and more cost effectively. All networks run into some difficulty at times. Quareo can reduce a six hour troubleshooting hunt down to three minutes, because it will show exactly what's changed.

Quareo and CPID technology has several benefits in the way of ROI, especially in reduced operational expenses. Operations personnel understand that there is currently an extraordinary amount of time spent documenting and troubleshooting the network. There is much poor data that exists from legacy networks and legacy management systems that can never be recorded and condensed in a way that CPID would manage automatically. So over the course of a very short period of time, ROI is realized just in terms of man hours and operational costs. In addition, anyone who runs a remote data center or NOC operation would have such an increased visibility into the network, that they could manage it, and manage assets in that network in such a way as to immediately realize operational benefits as well.

Contact: Quareo_Asia@te.com

Resources

Video: Learn about CPID Technology
Video: Learn about CPID Technology
Learn about the revolutionary connection point identification technology that brings managed connectivity to the physical layer of the network.
Watch Video
Take the Virtual Tour
Take the Virtual Tour
Take the Virtual Tour and see Quareo products inside a data center.
Take Tour
This list is temporary. The list will not be viewable on another computer and will be deleted within 30 days.

If your browser cookies are cleared, your temporary list will be lost. You can save this list and get all of the My Part List features by becoming a registered user of the TE web site.