• English

New Product: Multi-Channel Photocontrol Receptacle

02/20/2014

TE Connectivity launches the new ANSI C136.41 compliant Dimming Receptacle and spring leaf contacts providing an electrical and mechanical interconnection between an ANSI C136.41-2013 photo control cell and luminaire.

Product Features

Applications

Documentation & Additional Information




TE CONNECTIVITY UNVEILS ADVANCED MULTI-CHANNEL

PHOTOCONTROL RECEPTACLE
-- Innovative Receptacle Offers Increased Energy Efficiency and Progressive Dimming Capabilities –

DARMSTADT, Germany – 20 February, 2014 – TE Connectivity (TE), a world leader in connectivity, announces its innovative ANSI C136.41 compliant solution for the electrical and mechanical interconnection between a photocontrol cell and a street lighting luminaire. TE Connectivity is a pioneer in elegant interconnects that seamlessly integrate controls and transmit power and data across multiple building systems to enable optimal performance on every level.

The ANSI C136.41 compliant dimming receptacle along with the mating spring leaf contacts provide increased energy efficiency while expanding the dimming capabilities within streetlights.  Ideal for outdoor commercial and utility lighting, the ANSI C136.41 dimming receptacle is pre-configured with wire leads to allow for ease of integration into a new or existing outdoor lighting fixture.

 

The receptacles incorporate two or four signal connections along with the standard, proven ANSI C136.10 compliant twist-lock power connections that provide one or two channel photocell dimming capabilities within street lights. Mating spring leaf contacts are available for customer-designed photocontrol assemblies. Ample documentation is available to enable easy spring leaf contact integration into customer designs.

“The ANSI C136.41 compliant receptacle enables dimming capabilities and more intelligent controls in street lighting that ultimately reduce energy costs,” says Alex Hunt, product manager, TE Intelligent Buildings. “The receptacles provide a standardized interface that facilitates flexible, unparalleled control of street lighting when used with new or soon-to-be-released photo control modules.”

The ANSI C136.41 dimming receptacle is available with 105° C and 150° C rated wire insulation for various temperature graded luminaires. The receptacles meet dimensional requirements for ANSI C136.41-2013, as well as ANSI C136.10. There are two mechanical versions of the receptacles offered to manufacturers: a 5 position with three power contacts and two dimming contacts, and a 7 position with three power contacts and four dimming contacts. The power contacts can withstand voltages up to 480VAC/DC, and the dimming contacts up to 1A 600VAC/DC.

For more information on the ANSI C136.41 dimming receptacle, contact the Product Information Center at 1-800-522-6752 or visit the product overview page.

 

ABOUT TE CONNECTIVITY

TE Connectivity (NYSE: TEL) is a $13 billion world leader in connectivity. The company designs and manufactures products at the heart of electronic connections for the world’s leading industries including automotive, energy and industrial, broadband communications, consumer devices, healthcare, and aerospace and defense. TE Connectivity’s long-standing commitment to innovation and engineering excellence helps its customers solve the need for more energy efficiency, always-on communications and ever-increasing productivity. With nearly 90,000 employees in over 50 countries, TE Connectivity makes connections the world relies on to work flawlessly every day. To connect with the company, visit: www.TE.com.

 

 

Contacts:

 

Media Relations:

DeAnna Halewski

+1 (717) 652-0100 x210

dhalewski@sacunas.net

 

Venishree Mayer

+49 6151 607-1740

venishree.mayer@te.com

 

 

Product Communications:

Alex Hunt III

+1 (717) 986-5911

ahunt@te.com   

 

 

© 2014 TE Connectivity Ltd. family of companies. All Rights Reserved

This list is temporary. The list will not be viewable on another computer and will be deleted within 30 days.

If your browser cookies are cleared, your temporary list will be lost. You can save this list and get all of the My Part List features by becoming a registered user of the TE web site.