• English

New Product: INTRODUCING THE NEW UV-SCE MARKER SLEEVE FOR CABLE IDENTIFICATION IN HARSH UV AND WEATHER CONDITIONS

12/19/2012

TE Connectivity’s UV-SCE Marker Sleeves are the latest solution to identify wires and cables where extreme resistance to ultraviolet (UV) and harsh weather conditions are required.

Product Features

Applications

Documentation & Additional Information




December 19, 2012 – TE Connectivity, one of the world’s leading technology partners for railway companies, has developed the rugged wire and cable UV-SCE marker sleeve. This innovative solution preserves the integrity of sleeve markings on wires, cables and tubes outdoors under prolonged and extreme exposure to ultraviolet (UV) and harsh weather conditions.

The addition of the UV-SCE marker sleeve to the TE cable identification portfolio is in response to industry demand for applications within wire and cable environments where resistance to extreme UV and weather conditions is essential. This new product is well suited to applications within electrical, voice, data, video and outdoor security systems, addressing the needs of the Solar, Telecom (Networks), Offshore, Marine and Petrochemical industries.

The assembled and configured heat shrinkable UV-SCE marker sleeves provide outstanding physical performance, mark permanence and excellent legibility, ensuring long-term, outstanding performance of the TE cable identification service. Even after more than 25,000 hours of UV and moisture exposure, the long-lasting marker sleeve will not crack, chalk or fade, playing a vital role in the prevention of system failures. TE Connectivity developed and tested the marker sleeve to meet the highest standards in the industry, reinforcing TE’s position as a leader of innovation in the cable identification industry.

“As many industries look for the solution to a longstanding problem, TE has worked closely with our customers to develop the innovative UV-SCE marker sleeve," emphasized Peter Van Loo, General Manager of TE Rail. "This product and its applications address the need for cable identification systems that withstand harsh conditions, providing the market with the system solution that is required.”

For more information on TE’s UV-SCE marker sleeve, please contact your local TE Product Information Center or visit www.te.com/cable-identification

 

 

TE Connectivity, TE (logo) and TE connectivity (logo) are trademarks.

 

 

Contact:

Media Relations:

Wesley Gilbert

+44 1793572162

wesley.gilbert@te.com

 

Product Communications:

Julio Sevcik

+44 1793572080

julio.sevcik@te.com

 

 

 

 

 

 

 

About TE Connectivity

TE Connectivity (NYSE: TEL) is a $13 billion world leader in connectivity. The company designs and manufactures products at the heart of electronic connections for the world’s leading industries including automotive, energy and industrial, broadband communications, consumer devices, healthcare, and aerospace and defense. TE Connectivity’s long-standing commitment to innovation and engineering excellence helps its customers solve the need for more energy efficiency, always-on communications and ever-increasing productivity. With nearly 90,000 employees in over 50 countries, TE Connectivity makes connections the world relies on to work flawlessly every day. To connect with the company, visit www.te.com/.

 

 

This list is temporary. The list will not be viewable on another computer and will be deleted within 30 days.

If your browser cookies are cleared, your temporary list will be lost. You can save this list and get all of the My Part List features by becoming a registered user of the TE web site.