• English

New Product: New Push-Push SIM Connector Ideal For Multi-Card and Thinner Mobile Devices

07/10/2012

In response to the surging demand for multi-card mobile devices, TE Connectivity (TE) today launched its latest push-push SIM connector, featuring dual-slanted contacts that enhance stable connection and a super low profile design that enables sleeker product design.

Product Features

Applications

Documentation & Additional Information




SHANGHAI, China – July 10, 2012 –In response to the surging demand for multi-card mobile devices, TE Connectivity (TE) today launched its latest push-push SIM connector, featuring dual-slanted contacts that enhance stable connection and a super low profile design that enables sleeker product design – ideal for handset, tablet, personal GPS, laptop, ultrabook and server applications.

According to a market survey by GfK Market Research in 2011, multi-SIM use is set to grow exponentially, especially in newer and more emerging markets. “The multiple SIM facilitates the consumer-lead desire to utilize different tariffs throughout the week, depending on time and usage,” the report said [1].

"With its innovative design and quality construction, the new push-push SIM connector is our solution to the growing market demand for multi-card devices," said Youichi Kashiwa, product general manager, TE Consumer Devices. “TE has worked closely with leading mobile device manufacturers in the development and launch of this new product." The smooth push-push mechanism makes it easier for users to eject a SIM card, while the dual slanted contact design helps avoid contact jams from hooking housing components underneath and provides better mating performance during drop test.”

On the other hand, TE’s new push-push SIM connector is an ideal solution for slim mobile devices. The super low profile design provides connector height of only 1.4mm, which is 25% thinner than existing products and significantly helps reduce the height of end devices.

Consumers also yearn for a more polished user experience. TE's new push-push SIM connector features a card detect switch that enables hot swap and a wider card slot compatible with all SIM cards. In addition, the connector’s half-moon shape opening strengthens EMI protection. Extra open space at the front side of the housing helps prevent finger cuts when inserting or extracting the card.

TE's new push-push SIM connector meets industrial standards such as European Telecommunications Standards Institute (ETSI), ISO and GSM. For more information, please visit: http://www.te.com/products/simcardconnectors-PR.


[1] Multi SIM phenomenon continues in emerging mobile markets
>http://www.gfkrt.com/news_events/market_news/single_sites/007260/index.en.html

This list is temporary. The list will not be viewable on another computer and will be deleted within 30 days.

If your browser cookies are cleared, your temporary list will be lost. You can save this list and get all of the My Part List features by becoming a registered user of the TE web site.

Your notes will be stored and associated with this part.

Save
Cancel

Create a New List

Create
Cancel

Confirm Part Removal

This part will be removed from your list:

Remove Part
Cancel

Confirm Note Removal

Your note will be removed from your part.

Remove Note
Cancel